Schematic Library for MC9S12DG128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Schematic Library for MC9S12DG128

2,371 Views
ketankulkarni
Contributor I

Hello,

 

I am designing using MC9S12DG128 and would like to use Eagle for the schematic. I am unable to find any library for this controller. Can somebody point me an ready-made schematic library for this controller? Thanks!

 

Regards,

Ketan

Labels (1)
0 Kudos
Reply
3 Replies

2,029 Views
RadekS
NXP Employee
NXP Employee

Hi Ketan,

Typically we offer schematic symbols and footprint in Orcad/Allegro format at product details page. For example:

www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=S9S12GA240F0VLL

Unfortunately S12DG128 is older MCU and it seems that these data are not available on web site.

Could you please specify exact part number or at least package version (LQFP 112 or QFP 80)?

I could look into our system whether such symbol is available.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,029 Views
rayhall
Contributor V

Radek,

Sorry it was not deleted. I had the wrong discussion...

Ray.

0 Kudos
Reply

2,029 Views
rayhall
Contributor V

Radek,

Why was my reply deleted ?

Ray.

0 Kudos
Reply