MC9S12C128 SPI to SD Card with FAT file system.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12C128 SPI to SD Card with FAT file system.

1,326 Views
tnriley
Contributor III

I am trying to interface an MC9S12C128 controller SPI interface with an SD Card with FAT file system. Has anyone had success with this or know of examples that exist?

Labels (1)
0 Kudos
Reply
2 Replies

1,022 Views
rayhall
Contributor V

Hello Tim,

I also will need a driver for the MMC_SD card and FAT system.

I have just converted code written for the Atmel AVR to S12G128. The project compiles without errors, but I do not have a way to test it at the moment. Maybe you could do this.

Ray.

0 Kudos
Reply

1,022 Views
RadekS
NXP Employee
NXP Employee

Hi Tim,

I am afraid that currently we do not know about such example code.

There is Universal Serial Bus Card Reader Reference Design (DRM065) for S12UF32

http://www.freescale.com/products/archived/universal-serial-bus-card-reader-reference-design:RDHCS12...

However S12UF32 have directly SDHC controller module for access to SD card.

FAT file system is described in fatgen103.pdf file – please use your favourite search engine for download this file.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply