Schematic Library for MC9S12DG128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Schematic Library for MC9S12DG128

1,761件の閲覧回数
ketankulkarni
Contributor I

Hello,

 

I am designing using MC9S12DG128 and would like to use Eagle for the schematic. I am unable to find any library for this controller. Can somebody point me an ready-made schematic library for this controller? Thanks!

 

Regards,

Ketan

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,419件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Ketan,

Typically we offer schematic symbols and footprint in Orcad/Allegro format at product details page. For example:

www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=S9S12GA240F0VLL

Unfortunately S12DG128 is older MCU and it seems that these data are not available on web site.

Could you please specify exact part number or at least package version (LQFP 112 or QFP 80)?

I could look into our system whether such symbol is available.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,419件の閲覧回数
rayhall
Contributor V

Radek,

Sorry it was not deleted. I had the wrong discussion...

Ray.

0 件の賞賛
返信

1,419件の閲覧回数
rayhall
Contributor V

Radek,

Why was my reply deleted ?

Ray.

0 件の賞賛
返信