SENT Transmitter channels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SENT Transmitter channels

Jump to solution
1,710 Views
UmaMaheswaraReddy
Contributor IV

Hi,

In S12ZVC micros observed only one SENT TX module. If we need 4/more seperate sent channels in a single micro, how can we accommodate these types of situations?

 

From the below NXP link details my understanding is without actual SENT transmitter we can transmit SENT pulse patterns using below S32K144 example code. I am unable to understand below link attached code.

 

https://community.nxp.com/t5/S32K-Knowledge-Base/Uart-to-SENT-protocol-transmitter/ta-p/1129291

 

Do we have similar above link example code for S12ZVC micros. I have S12ZVC - DEVKIT EVB. I want to implement 4 SENT TX separate channels. In S12ZVC micros I observed only one SENTTX. Do we have any alternate option to accommodate this.

Do we have any micro/EVB with 4 separate SENT tx channels. 

0 Kudos
Reply
1 Solution
1,612 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @UmaMaheswaraReddy,

I can't confirm that it is possible to emulate SENT using TIM and PWM modules, because we don't have any demo or documentation in this regards. But yes, there are just two pins that are shared by the two modules.

 

BR, Daniel

 

View solution in original post

0 Kudos
Reply
5 Replies
1,683 Views
danielmartynek
NXP TechSupport
NXP TechSupport

HI @UmaMaheswaraReddy,

The S32K1xx series has FlexIO module that can be used to emulate the SENT protokol.

And for the newer S32K3xx we have also RTD FlexIO SENT Driver.

The S12Z MagniV series does not have FlexIO.

It would need to be emulated using GPIO or the TIM module, but we don't have any example / document for that.

 

Regards,

Daniel

0 Kudos
Reply
1,669 Views
UmaMaheswaraReddy
Contributor IV

Hi Daniel,

In S32K3xx series RTD, we observed FLEXIO SENT driver for SENT RX. Do we have SENT driver example for SENT TX?

 

UmaMaheswaraReddy_0-1727758590197.png

Thanks,

Y Uma Maheswara Reddy.

 

0 Kudos
Reply
1,637 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @UmaMaheswaraReddy,

Yes, you are right, this is just for the receiver.

I sent you one S32K1xx SENT TX FlexIO example privately.

Based on the information I have there should be an S32K3xx SENT TX FlexIO example next week.

 

BR, Daniel

0 Kudos
Reply
1,616 Views
UmaMaheswaraReddy
Contributor IV

Hi Daniel,

Thank you for the info. 

We can achieve SPC (SENT with Trigger) with the TIM and PWM (Without actual SENT transmitter). As per my understanding from the S12ZVC pins summary we have only two pins (PT2,PT3) with TIM and PWM combo. So maximum 2 SPC (SENT with trigger) we can implement, correct?

UmaMaheswaraReddy_0-1727944912660.png

 

I don't see any other pin supporting both PWM and TIM. Please correct me if I am wrong.

My requirement is I need to implement 6 SPC (SENT with trigger) in a single board.

Only PT2 and PT3 with TIM and PWM combination.

UmaMaheswaraReddy_3-1727945223305.png

 

UmaMaheswaraReddy_2-1727945184061.png

 

Thanks,

Y Uma Maheswara Reddy.

0 Kudos
Reply
1,613 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @UmaMaheswaraReddy,

I can't confirm that it is possible to emulate SENT using TIM and PWM modules, because we don't have any demo or documentation in this regards. But yes, there are just two pins that are shared by the two modules.

 

BR, Daniel

 

0 Kudos
Reply