S912zvml64 How to add LIN communication code separately

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912zvml64 How to add LIN communication code separately

1,408 Views
mine233
Contributor I

I am using s912zvml64 as the motor driver, but there is no LIN communication module in the motor code, so I can't realize LIN communication with the outside. So how can I add LIN communication code separately in s912zvml64? Is there any reference routine? Thank you.

0 Kudos
Reply
1 Reply

1,395 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

If you use our SW files for motor control then we do not modify them. They ar AS IS without modification support.

Please, look at the application note AN5122 Using NXP’s LIN Driver with the MagniV Family
https://www.nxp.com/docs/en/application-note/AN5122.pdf
The link to the SW you can find here:
https://community.nxp.com/t5/S12-MagniV-Microcontrollers/List-of-MagniV-and-S12-X-Application-notes/...

The LIN2.x and SAE J2602 Stack can be found in the part BSP, Drivers and Middleware at the page
https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

Probably the issue can be that there can be a collision in used timers so this should be considered in application.

Best regards,

Ladislav

0 Kudos
Reply