S912ZVML

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912ZVML

1,183 Views
madhuvatte
Contributor I

We are trying to get rid of TVS on the LIN bus of S912ZVML to reduce BOM costs even more. But is there any risks that doing it will fail ESD tests. Is the chip itself capable to sustain such harsh environment. What’s your suggestion? 

 

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

938 Views
RadekS
NXP Employee
NXP Employee

Hi Madhu,

It depends on your EMC (ESD) requirements.

The S12ZVML LIN was tested and pass through EMC test up to 6kV with Human Body Model (HBM) discharge.

Additionally, we specify also endurance against 6kV discharge according to IEC61000-4-2 with and without 220pF capacitor (R=330, C=150pF).

If your requirements are higher than this 6kV level, you will probably have to use external protection circuit like TVS.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply