S12ZVML PMSM Temperature Measure Source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12ZVML PMSM Temperature Measure Source

2,642 次查看
rzkity
Contributor II

Hello Everone!

   there is a problem relate to PMSM Sensorless Temperature Measure ,I can not understand following Program:

PMSM Meas_GetTemperature.png

Who can hellp me!

Thanks!

标记 (1)
0 项奖励
回复
3 回复数

2,396 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello[email protected],

Regarding the sensor, please refer to AN3624 S12X Temperature Sensor

https://www.nxp.com/docs/en/application-note/AN3624.pdf 

All MagniV S12Z MCU have the same sensor.

BR, Daniel

0 项奖励
回复

2,396 次查看
pachamatej
NXP Employee
NXP Employee

The internal temperature sensor is described in the Reference Manual. You can find some basic information e.g. on the page No.324, where the voltage of the temperature sensor is calculated as VHT(temp) = VHT(150DgC) – (150 – temp)*dVHT.

The slope dVHT is defined in Table B-1, row #13, typically 5.25 mV/DgC. The VHT(150DgC) is defined by the same table, row #14, as 2.4 V without any trimming.

VHT(temp) = 2.4 – (150 – temp)*5.25E-3

 

As an example, if the temp is 20 DgC, the voltage would be

VHT(temp) = 2.4 – (150 – 20)*5.25E-3 = 1.7175 V

 

Now, since the ADC is scaled to VDDA, typically 5 V, the full scale voltage (5 V) would mean

Temp = (VHT(temp) – 2.4 + 150*5.25E-3)/5.25E-3 = (5 – 2.4 + 0.7875)/5.25E-3 = 645.2381 DgC

However, this voltage should never occur since the chip would already burned out.

 

You may notice that the characteristics obtained the way above will be shifted as indicated below by orange Original line (ADC input relative, fitting the Frac16 format). To compensate this, a shift and slope needs to be added.

temp.png

The Original line can be expressed as:

VHT(temp) = 2.4 – (150 – temp)*5.25E-3

Scaled as:

VHT(temp) = (2.4 – (150 – temp)*5.25E-3)/5 = 0.48 – 0.1575 + 1.05E-3 * temp = ADC

ADC = temp * 1.05E-3 + 0.3225

To compensate, we would like to keep the maximum and have a zero output for zero temperature. Basically, we need to get from the input to the temperature through the Original line and then back to the input through the Compensated line.

Inverting the ADC function gives us:

Temp = (ADC – 0.3225) / 1.05E-3

The desired form of Compensated function is:

                ADC_comp = Temp / 645.2381 (the output is scaled to 1.0)

Combining these two functions in one, we get:

                ADC_comp = (ADC – 0.3225) / 1.05E-3 / 645.2381

To create a form of

                y = k * x + q

We simply need to extract the k and q values:

                k = 1/(1.05E-3 * 645.2381) = 1.476014

                q = - 0.3225/(1.05E-3 * 645.2381) = - 0.476014

These values are unfortunately outside of the Frac16 scale (outside of the -1.0 to 1.0 range). Therefore, let’s divide it by two (to be able to use bitwise shift).

                k = 0.738007

                q = - 0.238007

This operation is giving us the result divided by two. After the operation is done, we can multiply it again by two and get the compensated results.

 

The math concluded is:

ADC_comp = (0.738007 * (ADC) – 0.238007)*2

 

ptr->measured.f16Temp.raw = (tFrac16)(ADC1ResultList[0][1]);
ptr->measured.f16Temp.filt = MLIB_Mul_F16(ptr->measured.f16Temp.raw,FRAC16(0.73801));
ptr->measured.f16Temp.filt = MLIB_Sub_F16(ptr->measured.f16Temp.filt, FRAC16(0.23801));
ptr->measured.f16Temp.filt = MLIB_ShL_F16(ptr->measured.f16Temp.filt, 1);‍‍‍‍‍‍‍‍‍‍‍

 

The calculation provided in the meas_s12zvm.c in the GetTemperature() function should be as above (in case it is not yet corrected in the examples provided online).

2,396 次查看
rzkity
Contributor II

HI!

      Matej Pacha ,Thanks ! I understand the implications of this programs for your answer.But how do i calculate the temperature value via this variable.

please help me !

Thangks!!

0 项奖励
回复