S12ZVM128 EVB LIN communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVM128 EVB LIN communication

1,301 Views
bjhwang
Contributor I

Dear Sir or Madam,

I want to ask you question about the S12ZVM128 EVB LIN communication.

Currently I have two S12ZVM128 EVB boards and found two application notes(AN5201, AN5122).

But one is using S12ZVR32EVB for master, a S12ZVM128EVB for slave(AN5201), and the other one uses a S12ZVM EVB as master, S12VR64 EVB as slave(AN5122).
So I tried to mixed these it up, but it doesn't work.

Is there any application note that using two S12ZVM128 for LIN communication?

Thanks for reading

Best Regards

Tags (1)
0 Kudos
Reply
1 Reply

1,099 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Please refer to LIN2.x and SAE J2602 Stack (REV v4.5.9) which provides examples for both S12ZVML128 master and slave. See the user_guide file in the example folder.

Regards,

Daniel