S12ZVM128 EVB LIN communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVM128 EVB LIN communication

1,298件の閲覧回数
bjhwang
Contributor I

Dear Sir or Madam,

I want to ask you question about the S12ZVM128 EVB LIN communication.

Currently I have two S12ZVM128 EVB boards and found two application notes(AN5201, AN5122).

But one is using S12ZVR32EVB for master, a S12ZVM128EVB for slave(AN5201), and the other one uses a S12ZVM EVB as master, S12VR64 EVB as slave(AN5122).
So I tried to mixed these it up, but it doesn't work.

Is there any application note that using two S12ZVM128 for LIN communication?

Thanks for reading

Best Regards

タグ(1)
0 件の賞賛
返信
1 返信

1,096件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Please refer to LIN2.x and SAE J2602 Stack (REV v4.5.9) which provides examples for both S12ZVML128 master and slave. See the user_guide file in the example folder.

Regards,

Daniel