Hello,
Please check whether my understanding is correct about S12ZVM boost converter.
There are the specs about boost converter in S12ZVM as below,
VSUP boost turn on trip point V_BSTON : min 9.5V, typ 10.1V, max 10.6V
VSUP boost turn off trip point V_BSTOFF : min 9.75V, typ 10.3V, max 10.8V
My understanding is that:
--
1. These means
- when the VSUP becomes below V_BSTON, then the boost converter operates
and
- when the VSUP becomes above V_BSTOFF, then the boost converter doesn't operate.
2. Therefore, there is the hysteresis features and the boosted VSUP voltage has a ripple equivalent to V_BSTON-V_BSTOFF during boosting.
--
Is my understanding correct?
Best Regards,
Ikki
已解决! 转到解答。
Hi,
Well, yes, your understanding is correct. In case of low voltage on VSUP pin the boost converter operates (assuming that GBOE bit is set).
Not sure about the ripple. There are two capacitors in the external circuit of the boost converter. So the ripple should be reduced.
Regards,
iggi
Hi,
Well, yes, your understanding is correct. In case of low voltage on VSUP pin the boost converter operates (assuming that GBOE bit is set).
Not sure about the ripple. There are two capacitors in the external circuit of the boost converter. So the ripple should be reduced.
Regards,
iggi