S12ZVM boost converter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVM boost converter

ソリューションへジャンプ
2,054件の閲覧回数
ikkishingu
Contributor II


Hello,

 

Please check whether my understanding is correct about S12ZVM boost converter.

 

There are the specs about boost converter in S12ZVM as below,

VSUP boost turn on trip point V_BSTON : min 9.5V, typ 10.1V, max 10.6V

VSUP boost turn off trip point V_BSTOFF : min 9.75V, typ 10.3V, max 10.8V

My understanding is that:

--

1. These means

- when the VSUP becomes below V_BSTON, then the boost converter operates

and

- when the VSUP becomes above V_BSTOFF, then the boost converter doesn't operate.

 

2. Therefore, there is the hysteresis features and the boosted VSUP voltage has a ripple equivalent to V_BSTON-V_BSTOFF during boosting.

--

 

Is my understanding correct?

 

Best Regards,

Ikki

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,900件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

Well, yes, your understanding is correct. In case of low voltage on VSUP pin the boost converter operates (assuming that GBOE bit is set).

Not sure about the ripple. There are two capacitors in the external circuit of the boost converter. So the ripple should be reduced.

Regards,

iggi

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,901件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

Well, yes, your understanding is correct. In case of low voltage on VSUP pin the boost converter operates (assuming that GBOE bit is set).

Not sure about the ripple. There are two capacitors in the external circuit of the boost converter. So the ripple should be reduced.

Regards,

iggi

0 件の賞賛
返信
1,900件の閲覧回数
ikkishingu
Contributor II

Dear iggi,

Thank you for your information!

ikki

0 件の賞賛
返信