S12ZVM PMF internal signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12ZVM PMF internal signal

跳至解决方案
2,449 次查看
ikkishingu
Contributor II

Hello,

I have a question about S12ZVM PMF internal signal.

I refer S12ZVM RM rev2.11.

There is the description on Chapter15(PMF) that

"pmf_reload_is_async" serves as a qualifier to the PMF reload event signal "pmf_reloada".

On the other hand, there is another description on Chapter1 Figure 1-9. Internal Control Loop Configuration

that "reload" and "async_reload" signals outputs from PMF modules.

I can understand two patterns as follows.

1) "reload" = "pmf_reloada"

    "async_reload" = "pmf_reload_is_async"

2) "reload" = "pmf_reloada"

    "async_reload" = "pmf_reloada" ^ "pmf_reload_is_async" (logical conjunction)

Which is correct?

Best Regards,

Ikki

0 项奖励
回复
1 解答
2,171 次查看
RadekS
NXP Employee
NXP Employee

Hi Ikki,

I agree, that these internal signals descriptions in RM are quite confusing.  

 

The pmf_reloada signal is routed into PTU module. Therefore:

"reload" signal = "pmf_reloada" signal

 

The "pmf_reload_is_async" signal is also routed into PTU module. Therefore:

"async_reload" signal = "pmf_reload_is_async" signal

 

The pmf_reloada signal is generated at specified PWM opportunity (see chapter 15.4.12.3 Load Frequency) = at a start of control loop cycle.

The pmf_reload_is_async signal is generated when async_event (named also “commutation_event”, generated by TIM0_OC0) is detected.

 

If the PTU is enabled the reload and async_reload events are immediately passed through to the ADC and GDU modules.

 

If the restart is enabled (RSTRTx=1), the commutation event generates both “PWM reload event” and “PWM reload-is-asynchronous event” simultaneously except the case when the asynchronous event and generated PWM reload event occur in the same cycle (only “PWM reload event” is generated).

 

The PWM restart at commutation event is used for BLDC Six-Step Commutation driving (for both Hall/sensorless).

For example:

  PMFENCA_RSTRTA = 1;         // 1 = PWM restart at commutation event‍‍

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,172 次查看
RadekS
NXP Employee
NXP Employee

Hi Ikki,

I agree, that these internal signals descriptions in RM are quite confusing.  

 

The pmf_reloada signal is routed into PTU module. Therefore:

"reload" signal = "pmf_reloada" signal

 

The "pmf_reload_is_async" signal is also routed into PTU module. Therefore:

"async_reload" signal = "pmf_reload_is_async" signal

 

The pmf_reloada signal is generated at specified PWM opportunity (see chapter 15.4.12.3 Load Frequency) = at a start of control loop cycle.

The pmf_reload_is_async signal is generated when async_event (named also “commutation_event”, generated by TIM0_OC0) is detected.

 

If the PTU is enabled the reload and async_reload events are immediately passed through to the ADC and GDU modules.

 

If the restart is enabled (RSTRTx=1), the commutation event generates both “PWM reload event” and “PWM reload-is-asynchronous event” simultaneously except the case when the asynchronous event and generated PWM reload event occur in the same cycle (only “PWM reload event” is generated).

 

The PWM restart at commutation event is used for BLDC Six-Step Commutation driving (for both Hall/sensorless).

For example:

  PMFENCA_RSTRTA = 1;         // 1 = PWM restart at commutation event‍‍

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,171 次查看
ikkishingu
Contributor II

Hello Radek,

Thank you for your reply and I am sorry for the delay in my response.

From your comment, I understand 1) is correct as proper understanding.

Best Regards.

Ikki