S12ZVL: how to sync ADC with PWM rising edge

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL: how to sync ADC with PWM rising edge

1,804 Views
keli
Contributor I

Hi, there,

 

I am using S12ZVL to control a brushed DC motor. I would like to read bus current (through ADC) after the rising edge of the PWM. Any suggestion. Sample code will be appreciated.

 

Thanks, Ke

Labels (1)
0 Kudos
Reply
3 Replies

1,529 Views
RadekS
NXP Employee
NXP Employee

Hi Ke,

You could use ETRIG0 input as Trigger Event signal.

See example code in attachment.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,529 Views
kelimagna
Contributor I

Hi, Radek,

Thanks for the code. I am using 32 QFN, which doesn't have PP6. I am thinking to config PAD5 as input and direct-connect it with PP1 (my PWM pin). My concern is the PWM signal slope. Does it make sense?

Thanks, Ke

0 Kudos
Reply

1,529 Views
RadekS
NXP Employee
NXP Employee

Hi Ke,

In that case, external connection is probably best way.

PWM signal slope will depend on load which you connect to PP1 pin. Simple connection to PAD5 should have minimal impact.

If you will use PAD5, please enable digital input buffer by DIEN_DIENAD5 bit.

Optionally you could enable port P interrupt and triggering ADC by “ADC0FLWCTL_TRIG = 1;” command inside Port P interrupt routine. However this approach adds additional overhead for CPU and increase delay between PWM edge and ADC trigger event. Enter into interrupt routine takes some time (several bus clock cycles) and this time delay isn’t deterministic because CPU have to finish current instruction prior enter into interrupt routine.

On other side, solution with port interrupt allows to you drive time between PWM edge and ADC trigger event by software. Solution with ETRIG0 needs external circuit (or some additional routing to timer module) for driving time delay between PWM edge and ADC trigger event.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply