S12ZVL ACLK clock deafault value and COP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12ZVL ACLK clock deafault value and COP

跳至解决方案
2,290 次查看
charudattaingal
Contributor IV

Dear Team,

 

I want to know the default value of ACLK clock available in S12ZVL controller .

It is good to have if I get example of watchdog timer for S12zvl controller.

 

 

Thanks & Regards,

Charudatta

 

 

L&T Technology Services Ltd

 

www.LntTechservices.com<;http://www.lnttechservices.com/>

 

This Email may contain confidential or privileged information for the intended recipient (s). If you are not the intended recipient, please do not use or disseminate the information, notify the sender and delete it from your system.

标签 (1)
0 项奖励
回复
1 解答
2,069 次查看
RadekS
NXP Employee
NXP Employee

Hi,

This information is directly from MC9S12ZVL Family Reference Manual Rev. 1.04

Please look at chapter A.2.1 VREG Electrical Specifications (page 685), parameter 7,

Trimmed ACLK output frequency, typical value fACLK=20kHz.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,069 次查看
RadekS
NXP Employee
NXP Employee

Hi,

Nominal value of ACLK is 20kHz.

ACLK frequency is divided by 2 when ACLK is selected as clock source for watchdog:

ACLK.png

So, 10kHz is source clock frequency for COP watchdog.

Minimum timeout (CPMUCOP_CR=0x01, CPMUCLKS _COPOSCSEL1=1) is 2^7*(1/10kHz)=12,8ms

Maximum timeout (CPMUCOP_CR=0x07, CPMUCLKS _COPOSCSEL1=1) is 2^17*(1/10kHz)= 13,1072s

Note: ACLK frequency could be trimmed by modifying CPMUACLKTR register value. Note: After reset a value is automatically loaded again from the Flash memory.


I hope it helps you.


Have a great day,
RadekS


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,069 次查看
charudattaingal
Contributor IV

Dear RadekS,

Thanks for answer. The value of ACLK is not mention in S12zvl datasheet .

May I know how you got  ACLK value.

Thanks & Regards

Charudatta

0 项奖励
回复
2,070 次查看
RadekS
NXP Employee
NXP Employee

Hi,

This information is directly from MC9S12ZVL Family Reference Manual Rev. 1.04

Please look at chapter A.2.1 VREG Electrical Specifications (page 685), parameter 7,

Trimmed ACLK output frequency, typical value fACLK=20kHz.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,069 次查看
charudattaingal
Contributor IV

Thank you very much

0 项奖励
回复