S12ZVC naming rules

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVC naming rules

3,072 Views
thulzh
Contributor III

My team are using the S12ZVC series but found out the S912ZVC64F0MLFR is not enough for the GPIO pin. When we tried to change to the 64-pin S12ZVC, we are confused with the exact name of our target S12ZVC product, which has 64pin and 64kB flash memory. Is that S912ZVC64F0VKH, similiar to the S912ZVC12F0VKH on the official DEVKIT-S12ZVC? 

Is there any naming rules pdf or link about this?

Tags (1)
0 Kudos
Reply
3 Replies

2,964 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The details about part number can be found in the Reference Manual rev 2.1 in "Appendix M Ordering Information" https://www.nxp.com/docs/en/reference-manual/MC9S12ZVCRMV1.pdf 

The S912ZVC64F0VKH has 64 KB flash and "KH" at the end means package option: 64 LQFP

The S912ZVC12F0VKH has 128 KB flash and package option: 64 LQFP 

I hope it helps.

If you have any related questions, please let me know.

Best Regards,

Diana

2,964 Views
kef2
Senior Contributor V

See Appendix M Ordering Information in S12ZVC RM/Datasheet.

s12z-ordering.png

You need to replace LF to KH in package option.

2,964 Views
thulzh
Contributor III

Thank you!

0 Kudos
Reply