help :some questions about the AN3275(S12 All-Access Bootloader)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help :some questions about the AN3275(S12 All-Access Bootloader)

1,836 Views
treasure
Contributor I

hi ,

 

1. the code below is from AN3275,the author want to erase Paged Memory of the block 0(except the page 0x3F):

------------------------------------------------------------------------------------------------------------------------------

PPAGE=0x3E;
  li16PageAddressPointer=0xBFFF;
  li16BootAddressPointer = 0xFFFF;
  while(PPAGE>li8Page)
  {
    if(*(uint8 *)(li16BootAddressPointer) != *(uint8 *)(li16PageAddressPointer))
    {
     /*
      * Erase Paged Memory
      */
      gi32FlashAddressH = PPAGE;
      for(gi32FlashAddressL=0xBF00;gi32FlashAddressL>=0x8000;gi32FlashAddressL-=0x200){
        gi16FlashDataCounter = 1;
        if (vfnFlash_Cmd(FErase))
        {
          vfnSCITxMsg(&gi8aFlashErrorMsg[0]);
          return;
        }
      }
      PPAGE--;
      li16PageAddressPointer = 0xC000;
      li16BootAddressPointer = 0x0000;
    }
    li16BootAddressPointer--;
    li16PageAddressPointer--;
    if(li16BootAddressPointer<0xF000){PPAGE = 0x36;} 
  }

------------------------------------------------------------------------------------------

but ,in my opinion ,the code below is enough for erase those flash:

----------------------------------------------------------------------------------------------------

PPAGE=0x3E;
  while(PPAGE>li8Page)
  {
      gi32FlashAddressH = PPAGE;
      for(gi32FlashAddressL=0xBF00;gi32FlashAddressL>=0x8000;gi32FlashAddressL-=0x200){
        gi16FlashDataCounter = 1;
        if (vfnFlash_Cmd(FErase))
        {
          vfnSCITxMsg(&gi8aFlashErrorMsg[0]);
          return;
        }
      }
      PPAGE--;
   }

---------------------------------------------------------------------------------------------------------------

could you tell me why the author add the other statement, thanks!

 

 

2.  it seems that the author want to write the user‘s reset vector to 0xEFFE,but it doesn’t work,could you help me to solve it ,thank you!

-----------------------------------------------------------------------------------------------------------------

      if(gi32FlashAddressL >= (1 - gi16FlashDataCounter))  //Reset Vector
      {
        if(!S19UpdatingLoader)
        {
          gi16FlashDataCounter--;
          gi16FlashDataCounter--;
          ResetVector = *(uint16 *)(&gi8aS19Buffer[gi16FlashDataCounter+4]);
        }
      }
     
      gi16FlashDataCounter >>= 1;
      /* A single S19 record line shouldn't be longer than 0x20 bytes*/
      li8Error = vfnFlash_Cmd(Program);
      gi8S19Status &= ~((1<<S19RxComplete)|(1<<S19RxOk));
     
      if (!--li8LineCounter)
      {
        SCI0DRL = '.';
        li8LineCounter = 0x20;
      }
     
    }
  }
  if (S19UpdatingLoader)
  {
    vfnSCITxMsg(&gi8UpdateLoaderMsg[0]);
    vfnpUpdateFn();
  }
  else
  {
    gi16FlashDataCounter=1;
    gi32FlashAddress = 0xEFFE;
    gi8FlashBlock = 0;
    gi16pFlashDataPtr = (uint16)&ResetVector;
    (void)vfnFlash_Cmd(Program);
  }

Labels (1)
0 Kudos
Reply
2 Replies

1,375 Views
treasure
Contributor I

My friend help me solve the second problem,the BDM cause it.

0 Kudos
Reply

1,375 Views
martingebov
Contributor II

I too do not understand why the above statement was added and why the reset vector has to be programmed seperately. Can you share if you have any idea ?

0 Kudos
Reply