S12ZVC Power supply Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC Power supply Issue

1,287件の閲覧回数
kiranbhat
Contributor III

Hi

I am using s12zvc evaluation board MC9S12zvc. Recently I lost three boards (Controller heating once supply is connected, No VDDA, VDDX and VDDC supply) and dont know the reason. There is no problem from the power supply side, I have given 12V supply to the board with Aplab Bench Supply. Is there any one having same issue or anybody cna suggest the possible reason for the chip failure.

ラベル(1)
0 件の賞賛
返信
1 返信

1,130件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi kiran,

When controller heating once supply is connected, it typically means that there is some short on board or MCU is damaged. MCU may be damaged by strong ESD or by some electrical issue – typically when we connect 12V signal to any of 5V inputs.

Unfortunately I am not sure what could be root cause in your case.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信