S12ZVC Power supply Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVC Power supply Issue

1,285 Views
kiranbhat
Contributor III

Hi

I am using s12zvc evaluation board MC9S12zvc. Recently I lost three boards (Controller heating once supply is connected, No VDDA, VDDX and VDDC supply) and dont know the reason. There is no problem from the power supply side, I have given 12V supply to the board with Aplab Bench Supply. Is there any one having same issue or anybody cna suggest the possible reason for the chip failure.

Labels (1)
0 Kudos
Reply
1 Reply

1,128 Views
RadekS
NXP Employee
NXP Employee

Hi kiran,

When controller heating once supply is connected, it typically means that there is some short on board or MCU is damaged. MCU may be damaged by strong ESD or by some electrical issue – typically when we connect 12V signal to any of 5V inputs.

Unfortunately I am not sure what could be root cause in your case.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply