S12ZVC CAN transmitter buffer is full

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12ZVC CAN transmitter buffer is full

2,022 次查看
cwtc
Contributor II

hello

   when i call the function byte MSCAN0_SendFrameExt(dword MessageID,byte FrameType,byte Length,const byte *Data),

it returns ERR_TXFULL,i check the register CANTFLG = 0x00,it means message duffer is full,so i don`t konw why buffers are all full?

360截图-29151610.jpg

   i conncet a kvaser CAN data analysis as the other node,and this is my Processor Expert configuration

360截图-29188801.jpg

thanks.

0 项奖励
回复
4 回复数

1,791 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

Now I have the only question. Is your CAN bus connected to another node. The CAN is not working when there is no acknowledge from other node.

Loop-back mode helps you to say the CAN peripheral is OK and something wrong is on the BUS or transceiver.

Best regards,

Ladislav

0 项奖励
回复

1,791 次查看
cwtc
Contributor II

hi lama,

now i found the reason,i forgot enable CAN Physical Layer control register,that`s the reason why loop-back mode runs without any problem but can`t send data to bus.

thanks again :smileyhappy:

0 项奖励
回复

1,790 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

there is nothing possible to say from your description. Is it immediate status at the beginning or it happens during Tx.

As a first approach for CAN debugging I use loop-back mode to be sure the CAN is correctly working at the MCU. Then I try to use it to communicate with other nodes. Sometimes I also use communication between two CANs at the same MCU without transceiver. (requires a few diodes and resistors) This approach then helps me to localize source of the issue easier.

So from the beginning.

1) Communication related: Have you read the error messages? Are you sure the last messages has been sent?

2) Setup related: What is the transceiver RxTx delay and line delay [us/m]?

I have attached an example code , uses 4MHz oscclk, CAN0 in loopback mode, data Tx/Rx are sent to SCI, 8bit, 9600bps.

Please , test only it is working to be sure the CAN peripheral is OK. (There are some dditional excel files as a part of the project attached, only as an example)

Best regards,

Ladislav

0 项奖励
回复

1,790 次查看
cwtc
Contributor II

hi lama,

    thank you for your example code,but my mcu is S12ZVC64,so there`s something wrong when i debug it.

    when i call the function MSCAN0_SendFrameExt at first three times,err=0,mcu try to find a empty buffer to send message.until all buffers are full, function returns error ERR_TXFULL,so i think messages hasn`t been sent.

360截图-6729727.jpg360截图-6752830.jpg

meanwhile,oscilloscope does not show any waveform from CAN_H or CAN_L

    by the way,i tried loop mode,call the same function,in this way it returned OK,so does it mean CAN peripheral is OK?

0 项奖励
回复