S12XEP100 PORTA7 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12XEP100 PORTA7 problem

1,586件の閲覧回数
dashuangshengds
Contributor II

S12XEP100  GPIO output is not follow the software control.

        I use PORTA7 as output. After my ECU power on, I  set the GPIO is high and the pin voltage is high. When the ECU run few hours, the PORTA7 pin voltage is 0V, not  high level. 

        So I check the PORTA register, the DDR and DATA is follow the design and not changed during the running. 

        I want to know, is there any other cause for this problem?  Thank you!

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,503件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

you do not describe port connections (load) and entire setup. Pin is open drain after reset.

Only brief suggestion, PUCR_PUPAE=1;

Best regards,

Ladislav

0 件の賞賛
返信

1,503件の閲覧回数
dashuangshengds
Contributor II

Hi, thank you reply!

0 件の賞賛
返信