S12XEP100 PORTA7 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12XEP100 PORTA7 problem

1,619 Views
dashuangshengds
Contributor II

S12XEP100  GPIO output is not follow the software control.

        I use PORTA7 as output. After my ECU power on, I  set the GPIO is high and the pin voltage is high. When the ECU run few hours, the PORTA7 pin voltage is 0V, not  high level. 

        So I check the PORTA register, the DDR and DATA is follow the design and not changed during the running. 

        I want to know, is there any other cause for this problem?  Thank you!

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,536 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

you do not describe port connections (load) and entire setup. Pin is open drain after reset.

Only brief suggestion, PUCR_PUPAE=1;

Best regards,

Ladislav

0 Kudos
Reply

1,536 Views
dashuangshengds
Contributor II

Hi, thank you reply!

0 Kudos
Reply