S12UB UNIVERSITY BOARD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12UB UNIVERSITY BOARD

3,570件の閲覧回数
alessandrochiru
Contributor I

I'm experiencing some troubles with S12UB (product codes: LFEBS12UB and LFEBS12UBLAB).

The stand-alone kit, provide 21 labs, to get started with 9S12 architcture.

 

The first lab (attached)  just provide the basic information to connect the debug12 module with the PC through HyperTerminal. I follow all instructions (baud=9600, 8 bits data, no parity, 1 stop bit, xon/xoff etc.), but instead of visualizing the d-bug12 bootloader, i just recive from serial port random ASCII characters.

 

I tried to change baud, connect in different ways the MODE pins, but i always get the same problem.

 

i don't have a serial port on my PC, but i emulate it wit a prolific USB-to-Serial properly configured.

 

I also don't have no idea, about what pin i have to connect with jumpers (if i have to do it).

 

Is there some specific instruction manual for S12UB?

Is it possible that data in FLASH/EEPROM memory are corrupted? how can i do to rewrite the d-bug12 program in the uC?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,282件の閲覧回数
pablomartin
Contributor I

I did the first 17 labs with this S12UB board but the Lab 18 says that is unfinished and under development. Is there any way to obtain this lab? Thx! iggi‌

0 件の賞賛
返信

3,282件の閲覧回数
iggi
NXP Employee
NXP Employee

Issue resolved by distributor replacing the board.

0 件の賞賛
返信