Reset pin on MC9S12XEQ pulls down for unknown reason

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset pin on MC9S12XEQ pulls down for unknown reason

ソリューションへジャンプ
1,370件の閲覧回数
programmer
Contributor I

Hello,

 

I've started writing code for the MC9S12XEQ.

The code resets the COP watchdog timer by writing 0x55 and 0xAA, but for unknown reason, the RESET pin pulls down for 1.5 ms every 50 milliseconds.

 

This is also happens whenever the debugger stops the MCU (which is logical, but it also happens when the debugger is not connected).

 

How can I keep the RESET pin always up?

 

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,263件の閲覧回数
kef
Specialist I

S12XE pulls RESET pin low when internal reset occurs. It could be illegal address reset, COP or clock monitor reset.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,264件の閲覧回数
kef
Specialist I

S12XE pulls RESET pin low when internal reset occurs. It could be illegal address reset, COP or clock monitor reset.

0 件の賞賛
返信