Relocating interrupt vector table for s12zvc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Relocating interrupt vector table for s12zvc

Jump to solution
7,685 Views
kiranbhat
Contributor III

Hi

I am using s12zca192 controller, i am finding diffculty in relocating interrupt vector table. There are some regidters like IVBR byt not clear of how to use it. I wanted an example of how to relocate interrupt vector table.

 

 

 

 

Regards

Kiran Bhat

Labels (1)
1 Solution
6,902 Views
RadekS
NXP Employee
NXP Employee

Hi Kiran,

I see 16byte shift in your table.

PortAD interrupt vector should be on address = Vector base + 0xF4.

The same way are shifted also other interrupt vectors.

I started my vector table from address 0xFFF610 and my table has 123 vectors.

When you start table without that offset (0x10), you table should contain 127 vectors (the last/first vector is reset vector).

Note: 128 x 4B vector size = 512B

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
6,899 Views
RadekS
NXP Employee
NXP Employee

I prepared for you very simple example project with relocated interrupt vector table into RAM/Flash.

See attachment.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,899 Views
kiranbhat
Contributor III

Hi Radek

Thanks for the example. But i have one issue, whichever interrupt is configured each time on Unimplemented section is executed. I am pasting the code (Not able to attach the project) please check and correct me where i am wrong.

/*****************************Mani.c**********************************************/

#include <hidef.h> /* for EnableInterrupts macro */

#include "derivative.h" /* include peripheral declarations */

//#include "VectorTable.h"

void BSP_PIM_HLUWAKE_Interrupt_Enable(void);

unsigned int i;

void main(void)

{

  //IVBR=(INT_VECTOR_TABLE_ADDR_IN_FLASH & 0xFFFFFE)>>8;

  IVBR = 0xFEC4;

  DDRP_DDRP0 = 1;

  DDRP_DDRP4 = 1;

  DDRP_DDRP5 = 1;

  PTP_PTP0 = 1;

  PTP_PTP4 = 1;

  PTP_PTP5 = 1;

  BSP_PIM_HLUWAKE_Interrupt_Enable();

 

  EnableInterrupts;

  /* include your code here */

  for(;;)

  {

   PTP_PTP0 = ~PTP_PTP0;

   for(i = 0; i< 20000; i++);

  }

}

void BSP_PIM_HLUWAKE_Interrupt_Enable(void)

{

    /*configure port AD for KWU feature*/

    DDRAD_DDRADL3 = 0;            /* Configure PAD3 as input */   

  DIENADL_DIENADL3 = 1;         /* Pin is configured as digital input */

  PERAD_PERADL3 = 0;            /* Enable Pull Device on PAD3 */

  PPSAD_PPSADL3 = 1;            /* Configure interrupt for Rising Edge */

  PIEAD_PIEADL3 = 1;            /* Enable Interrupt on PAD3 (KWAD3) */

}

/***************************** End Mani.c**********************************************/

/******************************VectorTable.c*****************************************/

/*

* VectorTable.c

*

*  Created on: Jun 29, 2016

*      Author: kiran.bhat

*/

#include "VectorTable.h"

//==============================================================================

// Unimplemented_ISR

//==============================================================================

interrupt void Unimplemented_ISR(void)

{ 

  //PTP_PTP5 = ~PTP_PTP5;

  //PIFADL_PIFADL3 = 1;

  asm NOP;   //place breakpoint here

}

interrupt void WakeUpISR(void)

{

  PIFADL_PIFADL3 = 1;

  PTP_PTP4 = ~PTP_PTP4;

}

/***************************** End VectorTable.c**********************************************/

/******************************VectorTable.h*****************************************/

/******************************End VectorTable.h*****************************************/

Regards

Kiran

0 Kudos
Reply
6,899 Views
kiranbhat
Contributor III

/******************************VectorTable.h*****************************************/

/*

* VectorTable.h

*

*  Created on: Jun 29, 2016

*      Author: kiran.bhat

*/

#ifndef VECTORTABLE_H_

#define VECTORTABLE_H_

#include "derivative.h" /* include peripheral declarations */

#define INT_VECTOR_TABLE_ADDR_IN_FLASH 0xFEC400

#define INT_VECTOR_TABLE_SIZE 123

//Please see prm linker file where we removed area with vector table from linker usage.

/* ISR prototype */

interrupt void WakeUpISR(void);

interrupt void Unimplemented_ISR(void);

//vector table defined in Flash

typedef void (*const tIsrFunc)(void);

/* Pack 3 byte pointers as 4 byte Interrupt Vector Table entries */

typedef struct

{

  byte padding;

  tIsrFunc address;

} InterruptTableEntry;

#define _VECTOR(v) {0xFFU, &v}

//Please replace aprropriate Unimplemented_ISR by implemented interrupt routine

//see Table 1-13. Interrupt Vector Locations in RM for more details

const InterruptTableEntry _InterruptVectorTable[INT_VECTOR_TABLE_SIZE] @INT_VECTOR_TABLE_ADDR_IN_FLASH = { /* Interrupt vector table */

  _VECTOR(Unimplemented_ISR),//0x00     VReserved123          

  _VECTOR(Unimplemented_ISR),//0x04     VReserved122         

  _VECTOR(Unimplemented_ISR),//0x08     VReserved121         

  _VECTOR(Unimplemented_ISR),//0x0C  VReserved120         

  _VECTOR(Unimplemented_ISR),//0x10     VReserved119         

  _VECTOR(Unimplemented_ISR),//0x14     VReserved118         

  _VECTOR(Unimplemented_ISR),//0x18     VReserved117         

  _VECTOR(Unimplemented_ISR),//0x1C     VReserved116         

  _VECTOR(Unimplemented_ISR),//0x20     VReserved115         

  _VECTOR(Unimplemented_ISR),//0x24     VReserved114         

  _VECTOR(Unimplemented_ISR),//0x28     VReserved113         

  _VECTOR(Unimplemented_ISR),//0x2C     VReserved112         

  _VECTOR(Unimplemented_ISR),//0x30     VReserved111         

  _VECTOR(Unimplemented_ISR),//0x34     VReserved110         

  _VECTOR(Unimplemented_ISR),//0x38     VReserved109         

  _VECTOR(Unimplemented_ISR),//0x3C  VReserved108         

  _VECTOR(Unimplemented_ISR),//0x40     VReserved107         

  _VECTOR(Unimplemented_ISR),//0x44     VReserved106         

  _VECTOR(Unimplemented_ISR),//0x48     VReserved105         

  _VECTOR(Unimplemented_ISR),//0x4C     Vsenttx              

  _VECTOR(Unimplemented_ISR),//0x50     Viic                 

  _VECTOR(Unimplemented_ISR),//0x54     VReserved102         

  _VECTOR(Unimplemented_ISR),//0x58     VReserved101         

  _VECTOR(Unimplemented_ISR),//0x5C     VReserved100         

  _VECTOR(Unimplemented_ISR),//0x60     VReserved99          

  _VECTOR(Unimplemented_ISR),//0x64     VReserved98          

  _VECTOR(Unimplemented_ISR),//0x68     VReserved97          

  _VECTOR(Unimplemented_ISR),//0x6C  VReserved96          

  _VECTOR(Unimplemented_ISR),//0x70     VReserved95          

  _VECTOR(Unimplemented_ISR),//0x74     VReserved94          

  _VECTOR(Unimplemented_ISR),//0x78     VReserved93          

  _VECTOR(Unimplemented_ISR),//0x7C     Vtim1ovf             

  _VECTOR(Unimplemented_ISR),//0x80     VReserved91          

  _VECTOR(Unimplemented_ISR),//0x84     VReserved90          

  _VECTOR(Unimplemented_ISR),//0x88     VReserved89          

  _VECTOR(Unimplemented_ISR),//0x8C     VReserved88          

  _VECTOR(Unimplemented_ISR),//0x90     Vtim1ch3             

  _VECTOR(Unimplemented_ISR),//0x94     Vtim1ch2             

  _VECTOR(Unimplemented_ISR),//0x98     Vtim1ch1             

  _VECTOR(Unimplemented_ISR),//0x9C  Vtim1ch0             

  _VECTOR(Unimplemented_ISR),//0xA0     VReserved83          

  _VECTOR(Unimplemented_ISR),//0xA4     VReserved82          

  _VECTOR(Unimplemented_ISR),//0xA8     VReserved81          

  _VECTOR(Unimplemented_ISR),//0xAC     VReserved80          

  _VECTOR(Unimplemented_ISR),//0xB0     Vportl               

  _VECTOR(Unimplemented_ISR),//0xB4     VReserved78          

  _VECTOR(Unimplemented_ISR),//0xB8     VReserved77          

  _VECTOR(Unimplemented_ISR),//0xBC     VReserved76          

  _VECTOR(Unimplemented_ISR),//0xC0     VReserved75          

  _VECTOR(Unimplemented_ISR),//0xC4     VReserved74          

  _VECTOR(Unimplemented_ISR),//0xC8     VReserved73          

  _VECTOR(Unimplemented_ISR),//0xCC  VReserved72          

  _VECTOR(Unimplemented_ISR),//0xD0     VReserved71          

  _VECTOR(Unimplemented_ISR),//0xD4     VReserved70          

  _VECTOR(Unimplemented_ISR),//0xD8     VReserved69          

  _VECTOR(Unimplemented_ISR),//0xDC     VReserved68          

  _VECTOR(Unimplemented_ISR),//0xE0     VReserved67          

  _VECTOR(WakeUpISR),        //0xE4     Vportad              

  _VECTOR(Unimplemented_ISR),//0xE8     VReserved65          

  _VECTOR(Unimplemented_ISR),//0xEC     Vhti                 

  _VECTOR(Unimplemented_ISR),//0xF0    Vapi                 

  _VECTOR(Unimplemented_ISR),//0xF4    Vlvi                 

  _VECTOR(Unimplemented_ISR),//0xF8    Vevddx               

  _VECTOR(Unimplemented_ISR),//0xFC    Vportp               

  _VECTOR(Unimplemented_ISR),//0x100    VReserved59          

  _VECTOR(Unimplemented_ISR),//0x104    VReserved58          

  _VECTOR(Unimplemented_ISR),//0x108    VReserved57          

  _VECTOR(Unimplemented_ISR),//0x10C  VReserved56          

  _VECTOR(Unimplemented_ISR),//0x110    VReserved55          

  _VECTOR(Unimplemented_ISR),//0x114    Vports               

  _VECTOR(Unimplemented_ISR),//0x118    Vcanphy0             

  _VECTOR(Unimplemented_ISR),//0x11C    VReserved52          

  _VECTOR(Unimplemented_ISR),//0x120    VReserved51          

  _VECTOR(Unimplemented_ISR),//0x124    VReserved50          

  _VECTOR(Unimplemented_ISR),//0x128    VReserved49          

  _VECTOR(Unimplemented_ISR),//0x12C    VReserved48          

  _VECTOR(Unimplemented_ISR),//0x130    Vbats                

  _VECTOR(Unimplemented_ISR),//0x134    VReserved46          

  _VECTOR(Unimplemented_ISR),//0x138    VReserved45          

  _VECTOR(Unimplemented_ISR),//0x13C  VReserved44          

  _VECTOR(Unimplemented_ISR),//0x140    Vcan0tx              

  _VECTOR(Unimplemented_ISR),//0x144    Vcan0rx              

  _VECTOR(Unimplemented_ISR),//0x148    Vcan0err             

  _VECTOR(Unimplemented_ISR),//0x14C    Vcan0wkup            

  _VECTOR(Unimplemented_ISR),//0x150    Vflash               

  _VECTOR(Unimplemented_ISR),//0x154    Vflasherr            

  _VECTOR(Unimplemented_ISR),//0x158    VReserved37          

  _VECTOR(Unimplemented_ISR),//0x15C    Vspi1                

  _VECTOR(Unimplemented_ISR),//0x160    VRAM_err             

  _VECTOR(Unimplemented_ISR),//0x164    Vacmp1               

  _VECTOR(Unimplemented_ISR),//0x168    Vacmp0               

  _VECTOR(Unimplemented_ISR),//0x16C  Vcpmuplllck          

  _VECTOR(Unimplemented_ISR),//0x170    Vcpmuosc             

  _VECTOR(Unimplemented_ISR),//0x174    Vadc0conv_compl      

  _VECTOR(Unimplemented_ISR),//0x178    Vadc0conv_seq_abrt   

  _VECTOR(Unimplemented_ISR),//0x17C    Vadc0err             

  _VECTOR(Unimplemented_ISR),//0x180    VReserved27          

  _VECTOR(Unimplemented_ISR),//0x184    VReserved26          

  _VECTOR(Unimplemented_ISR),//0x188    Vsci1                

  _VECTOR(Unimplemented_ISR),//0x18C    Vsci0                

  _VECTOR(Unimplemented_ISR),//0x190    Vspi0                

  _VECTOR(Unimplemented_ISR),//0x194    Vtim0paie            

  _VECTOR(Unimplemented_ISR),//0x198    Vtim0paaovf          

  _VECTOR(Unimplemented_ISR),//0x19C  Vtim0ovf             

  _VECTOR(Unimplemented_ISR),//0x1A0    Vtim0ch7             

  _VECTOR(Unimplemented_ISR),//0x1A4    Vtim0ch6             

  _VECTOR(Unimplemented_ISR),//0x1A8    Vtim0ch5             

  _VECTOR(Unimplemented_ISR),//0x1AC    Vtim0ch4             

  _VECTOR(Unimplemented_ISR),//0x1B0    Vtim0ch3             

  _VECTOR(Unimplemented_ISR),//0x1B4    Vtim0ch2             

  _VECTOR(Unimplemented_ISR),//0x1B8    Vtim0ch1             

  _VECTOR(Unimplemented_ISR),//0x1BC    Vtim0ch0             

  _VECTOR(Unimplemented_ISR),//0x1C0    Vrti                 

  _VECTOR(Unimplemented_ISR),//0x1C4    Virq                 

  _VECTOR(Unimplemented_ISR),//0x1C8    Vxirq                

  _VECTOR(Unimplemented_ISR),//0x1CC  Vsi                  

  _VECTOR(Unimplemented_ISR),//0x1D0    VReserved7           

  _VECTOR(Unimplemented_ISR),//0x1D4    VReserved6           

  _VECTOR(Unimplemented_ISR),//0x1D8    Vme                  

  _VECTOR(Unimplemented_ISR),//0x1DC    Vsys                 

  _VECTOR(Unimplemented_ISR),//0x1E0    Vswi                 

  _VECTOR(Unimplemented_ISR),//0x1E4    Vtrap                

  _VECTOR(Unimplemented_ISR),//0x1E8    Vspare               

};              

#endif /* VECTORTABLE_H_ */

/******************************End VectorTable.h*****************************************/

0 Kudos
Reply
6,903 Views
RadekS
NXP Employee
NXP Employee

Hi Kiran,

I see 16byte shift in your table.

PortAD interrupt vector should be on address = Vector base + 0xF4.

The same way are shifted also other interrupt vectors.

I started my vector table from address 0xFFF610 and my table has 123 vectors.

When you start table without that offset (0x10), you table should contain 127 vectors (the last/first vector is reset vector).

Note: 128 x 4B vector size = 512B

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,897 Views
kiranbhat
Contributor III

Hi Radek

Thank you for the support issue solved. But i am still not clear with mapping concept. How it works and how linking happens. If you dont mind can you please explain the concept.

Regards

Kiran Bhat

0 Kudos
Reply
6,899 Views
RadekS
NXP Employee
NXP Employee

Hi Kiran,

Sure, it is really simple.

I will explain vector fetch on example.

When API interrupt occurs, the CPU finish current instruction and the interrupt module calculates offset according to interrupt source. In this case, it is 0x100.

See Table 1-13. Interrupt Vector Locations.

The CPU simply takes IVBR register content, move it to left by 8 bits (IVBR contains upper 15 bits from vector base address) and adds 0x100 offset. For example IVBR=0xFFC4. So, vector base is 0xFFC400. After adding 0x100 offset, we will get address 0xFFC500. At this address is stored starting address of API_ISR routine.

So, CPU will push their registers on stack and jump into API_ISR routine.

When code in API_ISR routine ends, the RTI instruction (Return from Interrupt) will pull back CPU registers from the stack.

Note: The RTI instruction is added on the end of ISR automatically because we used “interrupt” keyword in ISR declaration.

Note: Every vector has 4 bytes despite on fact that only 3 bytes are used for ISR address. So, if we want to fill a table with pointers to interrupt routines, we have to add dummy/padding byte at the beginning of every ISR address.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------