Regarding PMF register write protection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding PMF register write protection

1,494 Views
pratibhasurabhi
Contributor V

Hi All,

I am referring the MC9S12ZVM-Family RM.

15.8.1.1 Register Write Protection, note mentions -

Make sure to set the write protection bit WP in PMFCFG0 after configuring
and prior to enabling PWM outputs and fault inputs.

Query is whether this write protect [WP] feature is used to avoid writing on those registers by user or to avoid spurious writes[ not from user code].

My understanding is that once these write protect registers are initialised in the Init sequence, they are not written over again.

Thank you in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,424 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

the note is a friendly warning. If you have read the description of the WP bit then you have seen the last and by my opinion critical sentence which says you that there is no place for mistake:

Write Protect— This bit enables write protection to be used for all write-protectable registers. While clear, WP
allows write-protected registers to be written. When set, WP prevents any further writes to write-protected
registers. Once set, WP can be cleared only by reset.

Best regards,

Ladislav

0 Kudos
Reply