Reg. MC9S12DJ64 Controller Programing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reg. MC9S12DJ64 Controller Programing

3,330 次查看
balajiprabhakar
Contributor I
Hi all,
 
I am using MC9S12DJ64 controller, but I am not sure of which pins must be used to program the controller.
 
Can anyone help me out.
 
With regards,
 
Balaji.
标签 (1)
0 项奖励
回复
3 回复数

1,845 次查看
Lundin
Senior Contributor IV
The BKGD pin is the only one needed, though the BDM pod will want to use the reset line too. And of course a signal ground.

Both the BKGD and the reset line need a pull-up of 10k or so.
0 项奖励
回复

1,845 次查看
balajiprabhakar
Contributor I
Thanks Lundin,
 
Can I use Multilink programer for programing the controller. If so can you please give me the pin details of the same.
 
with regards,
 
Balaji.
0 项奖励
回复

1,845 次查看
Lundin
Senior Contributor IV
The pinning is available in both the Multilink manual and the S12 manual.
0 项奖励
回复