About the communication between two MSCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the communication between two MSCAN

2,076 Views
lwjtutu
Contributor I
The MSCAN0 and MSCAN1 are used in the  project and the CPU's type is MC9S12XDP512.
 
They can work normally in the LOOPBAKE mode respectively. But when the MSCAN0 sends a  message to the MSCAN1 or the MSCAN1 sends a  message to the MSCAN0, neither of  them can receive the message. I don;t know why?
   I am a fresh user of the chip, so I don't know  where the mistake may hides.
 Hope the experienced  users to tell me the mistake.
0 Kudos
Reply
1 Reply

1,037 Views
Nabla69
Contributor V
Hello,

If you wish several msCAN modules to talk together, you should not use the LOOPBACK mode.

Cheers,
Alban.
0 Kudos
Reply