Questions of 9S12DP512 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions of 9S12DP512 MCU

1,194 Views
monstor
Contributor II

Dear all,

 

I have the following questions of DP512.

 

1. I would like to develop a power save mode in DP512. E.g. sleep-wake up periodically. Have DP512 any internal timer interrupt to do this?

2. How long can DP512 sleep and then wake up If I use a 16M oscillator.

 

Thanks a lot for your helping.

Labels (1)
0 Kudos
Reply
1 Reply

1,010 Views
Martin35804
NXP Employee
NXP Employee

Hi,

Check the reference manual for the DP512:

9S12DP512_ZIP MC9S12DP512 Data Sheet and Reference Manual, zip format. Covers also the MC9S12DT512, MC9S12DJ512, and MC9S12A512

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12D&fpsp=1&tab=Documentation_Tab

.

especially check the S12MSCANV2.pdf in the folder

Three low-power modes: sleep, power down, and MSCAN enable

for instance for the MSCAN TX error counter register is readable only in sleep mode and in initialization mode. You can find in reference manual:

“Read: only when in Sleep Mode (SLPRQ=1 and SLPAK=1) or Initialization Mode (INITRQ=1 and

INITAK=1)”

The duration of sleep mode depends from your setting of interrupt - wake up.

0 Kudos
Reply