Problems flashing S12ZVC192 with PEMICRO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems flashing S12ZVC192 with PEMICRO

Jump to solution
1,818 Views
braxton
Contributor II

hello, i'm having trouble flashing my s12zvc192 via codewarrior using a pemicro multilink universal. i get the following error:

Error executing task MC9S12ZVC192.
Error: command failed

 

the workspace log shows:

org.eclipse.core.runtime.CoreException: Unknown target type: com.freescale.cw.system.s12z.S12ZVC.MC9S12ZVCA192

 

 

i have flashed s12s in the past with this machine (win10) so i'm not sure what's up.

0 Kudos
Reply
1 Solution
1,805 Views
braxton
Contributor II

it was a broken JTAG cable.

View solution in original post

0 Kudos
Reply
1 Reply
1,806 Views
braxton
Contributor II

it was a broken JTAG cable.

0 Kudos
Reply