Problem with CodeWarrior USB TAP and Win 7.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with CodeWarrior USB TAP and Win 7.

跳至解决方案
6,639 次查看
miroslavmartise
Contributor I

Hello boys and girls,

 

I have got a huge problem with CodeWarrior USB TAP on my PC with Windows 7. At the moment I am developing some devices using DSP MC56F8037. If I want program this processor with CW USB TAP and 56800E Flash Programmer, this note appears: "CCCSClient::WriteMemoryDirect: Core not responding" and nothing is done. Before I  connected CW USB TAP with my computer for the first time, I had to install new driver for USB TAP, but it went without a hitch. Success! But when I decided to load my program into DSP, the error occured, I have already mentioned. I don´t know, what I should do with it. I have already controlled as many as 100 times SW and HW but I cannot still solve this problem. In my opinion, the core of this bad situation will be located in Windows 7. Can someone give me an advice to solve it?

I am sorry, my English is not good.

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
3,327 次查看
TICS_Fiona
NXP Employee
NXP Employee

Are you using stand-alone verion v1.2 of 56800E Flash Programmer? Please install  this CCS update in it:

https://community.freescale.com/docs/DOC-93785

If there's still any problem, please enter a service request from:

https://www.freescale.com/webapp/servicerequest.create_SR.framework

I will help you in the SR. Thanks.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,328 次查看
TICS_Fiona
NXP Employee
NXP Employee

Are you using stand-alone verion v1.2 of 56800E Flash Programmer? Please install  this CCS update in it:

https://community.freescale.com/docs/DOC-93785

If there's still any problem, please enter a service request from:

https://www.freescale.com/webapp/servicerequest.create_SR.framework

I will help you in the SR. Thanks.

0 项奖励
回复
3,327 次查看
mariannabuschle
Contributor II

Hi,

I have a similar problem.

I have CodeWarrior 7.3 installed and running fine in Win7 after the patch from AN4338

I have now tried to install the standalone flash programmer 1.2.

It erases the flash and then gives a "CCCSClient::WriteMemoryDirect: Core not responding" message.

I tried applying your patch but still without success...

Thank you

Marianna

0 项奖励
回复
3,327 次查看
miroslavmartise
Contributor I

Hello,

I tested it before several minutes and it works properly. Incredible!  Thanks very much!!

0 项奖励
回复