2 starting questions on S12 boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2 starting questions on S12 boards

ソリューションへジャンプ
1,061件の閲覧回数
mister_l
Contributor I

Hi,

I recently started learning microcontroller development. I had the change to obtain 2 S12 evaluation

boards. I succeeded in doing some 1st examples with CodeWarrior debugger. Though I have 2 starting

questions:

1) the book I am working with (M. Cady) is talking about a D-Bug12 monitor residing on S12. But it

    looks like this SW isn't installed. Am I correct that for some eval boards I need to install it myself?

    I guess chips for mass production won't have D-Bug12 installed neither?

2) what exactly does the abbreviation "POD" stand for? It seems to be a USB2BDM converter

    between PC host and eval board.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
956件の閲覧回数
kef2
Senior Contributor V

Hi

1) yes.yes,

2) right

Those days when there was no USB2BDM, but only some quite expensive LPT2BDM, it probably wasn't too chip to have extra MCU on evaluation board to serve as BDM adapter. So there was D-Bug12. Today it doesn't make a lot of sense to bother with Dbug-12. DEMO boards like this one have USB2BDM on board

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9S12XEP100

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
957件の閲覧回数
kef2
Senior Contributor V

Hi

1) yes.yes,

2) right

Those days when there was no USB2BDM, but only some quite expensive LPT2BDM, it probably wasn't too chip to have extra MCU on evaluation board to serve as BDM adapter. So there was D-Bug12. Today it doesn't make a lot of sense to bother with Dbug-12. DEMO boards like this one have USB2BDM on board

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9S12XEP100

0 件の賞賛
返信