Problem to communicate with UJA1023 LIN I/O Slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem to communicate with UJA1023 LIN I/O Slave

8,110 Views
jackson0
Contributor I

Hello,

I have a problem to communicate with a UJA1023 slave. C1-C3 conntected to GND.

I send from master: BREAK + SYNCFRAME(0x55) + 3C 60 06 B1 11 00 00 00 04 D2(CHECKSUM)

And then: BREAK + SYNCFRAME(0x55) + 7D (3D with Parity bits)

but after this the UJA1023 gives no Data for answer.

What did I wrong?

Regards,

Michael

Labels (1)
0 Kudos
Reply
1 Reply

7,738 Views
1602670702
Contributor I
Hello, UJA1023 input is what mean?How to set up in the program?thank you. SB SF 80 whats meaning ?why need UJA1023 input ? Input triggers an IO, UJA1023 how to inform the host, return the data?thank you can you give me a example?
0 Kudos
Reply