Port Pin Control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Port Pin Control

跳至解决方案
10,056 次查看
rayhall
Contributor V

I know this is very basic if you know the way to control the pins on ports. I am stuck.

 

DDRD = 0xFF;  // Set the pins as outputs

PORTD = 0xFF; // Turns on the pullups

 

How do you set PD0 low. This does not work PORTD_PDO = 0x00;

 

Ray.

标签 (1)
0 项奖励
回复
1 解答
9,741 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ray,

maybe I don't understand.

I just tested the code on my side, I can see portd bit0 at memory 0x0005 got toggled with

  PORTD_PD0=0x00;  //set output pin as low

  asm nop;

  PORTD_PD0=0x01;  //set output pin as high

see attached video.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
15 回复数
9,741 次查看
rayhall
Contributor V

I have it now working. I am not sure if there is a better way to control the pins. This works.

  PUCR |= 0x08; //set pull up on Port D

  DDRD_DDRD0=0x01;  // set direction as output

  for(;;) {

 
PORTD |= PORTD_PD0;
Delay_ms(2000);
PORTD = ~PORTD_PD0;
      
_FEED_COP(); /* feeds the dog */

  } /* loop forever */

It is weird how you must use PORT_PD0  and 0x01 is ignored.

Ray.

0 项奖励
回复
9,741 次查看
Martin35804
NXP Employee
NXP Employee

Hi,

to make the proper port off again try to and it with the neg. value of the port.

PORTD &= ~(PORTD_PD0);

9,741 次查看
rayhall
Contributor V

Martin,

I get nothing when using.

PORTD |= PORTD_PD0;

asm nop;

PORTD &= ~PORTD_PD0;

This works...

PORTD = 0x01;

asm nop;

PORTD = 0x00;

So does this...

PORTD |= (1<<0);

asm nop;

PORTD &= ~(1<<0);

They work correctly as long as I do not use my delay method. See reply to Zhang.

Ray.

0 项奖励
回复
9,741 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ray,

it is not  "must", I just do a quick test if  PORT_PD0 can function normal. you can modify the code as your requirement.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

Zhang,

it is not  "must", I just do a quick test if  PORT_PD0 can function normal. you can modify the code as your requirement.

It is not that I want to modify your example. It is that this did not work.

  PORTD_PD0=0x00;  //set output pin as low

  asm nop;

  PORTD_PD0=0x01;  //set output pin as high

I would have expected your example to work as that is what I have used with other MCU. I wish someone could explain what possible reason you cannot set the bits for the pins.

Ray.


0 项奖励
回复
9,742 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ray,

maybe I don't understand.

I just tested the code on my side, I can see portd bit0 at memory 0x0005 got toggled with

  PORTD_PD0=0x00;  //set output pin as low

  asm nop;

  PORTD_PD0=0x01;  //set output pin as high

see attached video.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

Zhang,

If I use this code I get this pattern on my oscilloscope. http://www.turbofast.com.au/tfbin/TEK0000.JPG which is correct.

PORTD |= (1<<0);

asm nop;

PORTD &= ~(1<<0);

If I use this code I get this pattern which is wrong. http://www.turbofast.com.au/tfbin/TEK0001.JPG

PORTD |= (1<<0);

Delay_us(1);

PORTD &= ~(1<<0);

For some reason my delay method is causing problems. This is its code.

#define F_BUS 50  // 50mHz

#define  LOOP_US    ((F_BUS*1000000/6000000)+1)

void Delay_us(unsigned short ms){

    unsigned short j, k;

    for(j=0;j<ms;j++){

        for(k=0;k<LOOP_US;k++){

        }

    }

}

Ray.

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

Sorry....My delay method is working correctly. The code should have another delay like this.

PORTD |= (1<<0);

Delay_us(1);

PORTD &= ~(1<<0);

Delay_us(1);

Sorry for all the confusion. Thank you all,  for your help.

Ray.

0 项奖励
回复
9,741 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ray,

please refer this code:

  PUCR = 0x08;  //set pull up

  DDRD_DDRD0=0x01;  // set direction as output

  PORTD_PD0=0x00;  //set output pin as low

  asm nop;

  PORTD_PD0=0x01;  //set output pin as high

 

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

Zhang,

I have found that you cannot set the pullup like this. PUCR = 0x08; It causes debug break point errors.

You have to use PUCR |= 0x08;

To set Port C and D pullups you cannot use PURC = 0x0C;

You have to do this...

PUCR |= 0x04;

PUCR |= 0x08;

I still cannot set the pins high or low, and need help with this. Why is such a basic thing so hard..

Ray.

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

Zhang,

I get a ILLEGAL_BP when I use the PURC = 0x08; and the pin does not change.

This is my test code,

  PUCR = 0x08; //set pull up

  DDRD_DDRD0=0x01;  // set direction as output

  for(;;) {

 

PORTD_PD0=0x00;  //set output pin as low
Delay_ms(2000);
PORTD_PD0=0x01;  //set output pin as high

;  

_FEED_COP(); /* feeds the dog */

  } /* loop forever */

This below does work...Why ?

   DDRD = 0x01;

  PORTD = 0x01;

  for(;;) {

      

     Delay_ms(2000);

     PORTD_PD0 = ~PORTD_PD0;

         

    _FEED_COP(); /* feeds the dog */

  } /* loop forever */

Ray.

0 项奖励
回复
9,741 次查看
iggi
NXP Employee
NXP Employee

Ray, what MCU do you use?

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

iggi,

I am using the 144 pin S12XEP100

Ray.

0 项奖励
回复
9,741 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

please post here your project. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
9,741 次查看
rayhall
Contributor V

Zhang,

Here is the project,

http://www.turbofast.com.au/tfbin/LCDtest.zip

Ray.

0 项奖励
回复