Please provide the Demo code for EVB9S12XEP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please provide the Demo code for EVB9S12XEP100

1,754 Views
zhide99
Contributor I


Hi everyone, I am a beginner for using the MC9S12XEP100. Now, I have a development board "EVB9S12XEP100" . Who can provide the DEMO codes for runing in the  board of  EVB9S12XEP100. Thank you.

Labels (1)
3 Replies

1,544 Views
RadekS
NXP Employee
NXP Employee

Hi 翔 田

In the attachment, you could find documents and examples from EVB9S12XEP100 CD.

More S12XE examples could be downloaded here:

https://community.freescale.com/docs/DOC-95116

or here:

https://community.freescale.com/docs/DOC-329209


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,544 Views
zhide99
Contributor I

Hi Radek Sestak,

         Thank you for your help. Can you  provide the driver of "uDART In-Circuit Debugger". My evaluation board is not connected to the PC by the "USB TO BDM INTERFACE".Because  the lack of driver for uDART In-Circuit Debugger. Thanks!

0 Kudos
Reply

1,544 Views
RadekS
NXP Employee
NXP Employee

Hi 翔 田,

Unfortunately, SofTec interface driver is not supported by 64bit OS.

Authors of this interface terminated cooperation with Freescale and henceforth they did not support this product.

There are possible solutions:

1.    Different BDM Interface. For example P&E Universal Multilink Interface: Universal Multilink Development Interface|NXP

2.    Different operational system. For example any 32bit windows.

3.    Install virtual PC, Windows XP Mode 32bit, Install CW, and drivers...

More details you can get from our application note AN3936 How to install and run Classic CodeWarrior products on 64-bit Windows 7 PC: http://www.nxp.com/files/soft_dev_tools/doc/app_note/AN3936.pdf

I would like to apologize for that problems, but it was not caused by our fault.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------