PGA Select Inputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PGA Select Inputs

1,318 Views
charudattaingal
Contributor IV

Hi All,

Currently I'm using register PGAINSEL[1:0] to select inputs for PGA.

 

 

10 PGA_IN0 is selected as input voltage (PGAIN).

 

11 PGA_IN1 is selected as input voltage (PGAIN).

 

 

Issue: The value getting as PGA output for the inputs given is getting skewed occasionally.

 

So I want to configure ADC option Bits to select the PGA inputs to solve this.

 

If I need to use  ADC option bit to select PGA inputs i.e.

 

ADC option bit[3:0] PGA input source selection

 

What are all the configurations to be made.

Can anyone help on this?

 

-Charudatta

Labels (1)
0 Kudos
Reply
1 Reply

1,199 Views
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

In attachment is simple ADC example code for S12ZVL.

So, for measuring PGA_IN0 and PGA_IN1 you may configure commands like:

#define PGA_ADC          0x0F      //See table Analog Input Channel Select in refernce manual

adc0_cmdlist[0] = CMD_SEL(norm)+ OPT(1)+INTFLG_SEL(0)+VRH_SEL(1)+VRL_SEL(1)+CH_SEL(PGA_ADC)+SMP(0x14);

adc0_cmdlist[1] = CMD_SEL(eolw)+ OPT(2)+INTFLG_SEL(1)+VRH_SEL(1)+VRL_SEL(1)+CH_SEL(PGA_ADC)+SMP(0x14);

Note: SMP(0x14) refers to longest sampling time = 24 ADC Clock Cycles

Unfortunately, I don't have S12ZVL64/S12ZVL96/S12ZVL128 board, for now, therefore, I cannot test it.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply