Why  the  mc9s12zvm128  microcontroller  is  easy  to  damage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why  the  mc9s12zvm128  microcontroller  is  easy  to  damage

1,157 次查看
pengweiyes
Contributor I

I am use the MC9S12ZVM128  microcontroller .

In the process of application I find the Mc9s12zvm128’s VBS0~VBS3 are  easy to damage, Circuit diagram is as follows:

148276_148276.pngpastedImage_0.png

标签 (1)
0 项奖励
回复
1 回复

1,037 次查看
RadekS
NXP Employee
NXP Employee

Hi 伟 彭,

I would like to recommend an optional RC filter to VBS pin (for all three phases) that it be used to avoid overshoot above the maximum voltage on VBS pin. The RC filter needs to be carefully designed in order not to influence the charging time of the bootstrap capacitor CBS.

Optional RC filter to VBS pin.png


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复