One shunt Sensorless  BLDC control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

One shunt Sensorless  BLDC control

1,982 Views
ahnjoseph
Contributor III

Can do s12zvl Sensorless BLDC controlcontrol with One shunt ?

If it can do How can use nxp LIB ?

Labels (1)
0 Kudos
Reply
2 Replies

1,798 Views
RadekS
NXP Employee
NXP Employee

Hi Ahn,

Unfortunately s12zvl is not directly designed for driving BLDC motor.

You will probably need external FET driver. Please look at hardware solution for older S12G family:

http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...

Or you could choose one of s12zvm family derivatives with gate drive unit module and drive BLDC motor directly. For more details, please look at:

http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,798 Views
ahnjoseph
Contributor III

Thanks your kindly mention of my question 

I know s12zvl is
not directly Motor control it must be with FET or IGBT

So, My question is
using just one shunt for FOC-sensorless BLDC MOTOR control with NXP LiB

Normally, Sensorless
control is using with 3-shuts or 2-shunts

Can s12zvl control Sensorless
BLDC motor with just one-shunt?

0 Kudos
Reply