Need information Regarding CAN interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need information Regarding CAN interface

1,398件の閲覧回数
pratayay123
Contributor III

Dear Team,

I Need the below information Regarding the CAN transceiver for MTRCKTSPNZVM128  (MC9S12ZVML128 MCU).

1.  Is there an Inbuild CAN transceiver is available for the MTRCKTSPNZVM128 development kit(MC9S12ZVML128 MCU).

2. is there any process document or workshop/tutorial available for CAN protocol for the MTRCKTSPNZVM128 development kit(MC9S12ZVML128 MCU).

3. If the inbuild CAN transceiver is not available in kit then what is the process to connect CAN for the MTRCKTSPNZVM128 development kit(MC9S12ZVML128 MCU).

4. Please share supporting documents for CAN protocol for NXP

 

Thanks,

Pratyay

0 件の賞賛
返信
1 返信

1,347件の閲覧回数
StanoA
NXP TechSupport
NXP TechSupport

Hello Pratayay,

There is the CAN driver IC on board connected to J8.
You can use the AN:
https://www.nxp.com/docs/en/application-note/AN4975.pdf
and CAN Protocol Standard:
https://www.nxp.com/docs/en/reference-manual/BCANPSV2.pdf
and attached SW example with calculators to build your application.
I think it could help you with your task.

Best Regards,

Stano.

0 件の賞賛
返信