LIN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN

3,583 Views
1023578211
Contributor I

Its been 2 weeks, and yet i cannot accomplish anything with the s12zvl32, because i cannot find any example on the internet, all the example links posted in this community related to the S12xxx are either expired , or doesn't exist ,

Labels (1)
0 Kudos
Reply
3 Replies

3,531 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The example for the S12ZVL32 is located in the LIN stack

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW-LIN2X-J2602-D 

However, the AN5122 Using Freescale’s LIN Driver with the MagniV Family can be useful:

https://www.nxp.com/docs/en/application-note/AN5122.pdf 

SW:

https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3Fcol... 

I hope it helps.

Best regards,

Diana

0 Kudos
Reply

3,265 Views
1023578211
Contributor I

Hi

Why is there an error in compiling code in CodeWarrior V10.7?

How to deal with it?

Description Resource Path Location Type
Could not open 'parameter file' 'E:\Freescale\CW\beifen\2020071603\FS11_FCP_New_Version\FLASH\burner.bbl' FS11_FCP_New_Version C/C++ Problem

 

 

0 Kudos
Reply

3,525 Views
1023578211
Contributor I

How to download Node Configuration Tool and LDF file and NPF file creation

0 Kudos
Reply