NXP BLDC Motor Controller - Improve Power Stage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP BLDC Motor Controller - Improve Power Stage

Jump to solution
3,736 Views
datamstr
Contributor II
Hello all,
 
I am looking to build a BLDC motor controller or modify one. The NXP reference boards are insufficient with the power stage current. The motor I have is 3 phase and intended for operation in roughly the 12 to 14 V dc range. The motor power rating is somewhere around 1.2 KW and I think the stall current is around 150 Amps. I am not sure what the average operating current is. Also, I think the design was for operation up to around 4,000 RPM and the motor design is 12 slots with 8 poles.
 
Any thoughts about using a NXP reference design and modifying the Power Output Stage to handle the motor I have?
 
I have the S12ZVML MINI-BRD Development Board for 3-phase sensorless BLDC and I have the S32k144 Eval board.
 
Here are my questions:
 
Should I try to modify the power stage of the S12ZVML-MINIBRD to drive my motor or should I look at the S32K144 Eval board since I need to modify the power stage anyway or should I do a design from scratch?
 
If I try to modify the S12ZVML-MINIBRD power stage, what changes need to be made for the sensorless feedback?
 
Thanks,
David
0 Kudos
Reply
1 Solution
3,711 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

the colleague of mine from an app group suggests following...

 

My sugestion is not to use https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

S12ZVML 3-phase BLDC/PMSM Evaluation Kit

The S12ZVML-MINIBRD evaluation board and the S12ZVML-MINIKIT evaluation kit are engineered for 3-phase BLDC and PMSM sensorless motor control applications.

 

but this one

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

S12ZVM high-current BLDC/PMSM Evaluation Board

The MCSXSR1CS12ZVM is an evaluation board engineered for 3-phase brushless direct current (BLDC) and permanent magnet synchronousmotor (PMSM) control in high-current applications

 

It is for higher power and there are also supporting documents and files.

 

Best regards,

Ladislav

View solution in original post

0 Kudos
Reply
2 Replies
3,712 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

the colleague of mine from an app group suggests following...

 

My sugestion is not to use https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

S12ZVML 3-phase BLDC/PMSM Evaluation Kit

The S12ZVML-MINIBRD evaluation board and the S12ZVML-MINIKIT evaluation kit are engineered for 3-phase BLDC and PMSM sensorless motor control applications.

 

but this one

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

S12ZVM high-current BLDC/PMSM Evaluation Board

The MCSXSR1CS12ZVM is an evaluation board engineered for 3-phase brushless direct current (BLDC) and permanent magnet synchronousmotor (PMSM) control in high-current applications

 

It is for higher power and there are also supporting documents and files.

 

Best regards,

Ladislav

0 Kudos
Reply
3,691 Views
datamstr
Contributor II

Thanks Ladislav!

I will take your suggestion and use the MCSXSR1CS12ZVM for my motor control solution.

David

0 Kudos
Reply