Multilink universal rev e cannot connect to S12ZVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multilink universal rev e cannot connect to S12ZVM

1,806件の閲覧回数
GTM
Contributor I

I recently bought a Multilink Universal Rev E. When I use Code Warrior to debug the code, it says that it cannot establish a connection with my S12ZVM development board.

0 件の賞賛
返信
2 返答(返信)

1,787件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

Please ensure that you selected correct port. Debugger-menu-HC12MultilinkCyclonePro-Communication-Port…

Please disconnect external loads connected to the board.

Please ensure that you don’t have open more than one debugger window.

Please ensure that MCU is correctly powered.

Check correct connection of the multilink to the connector. (I often connect it in opposite direction to the BDM connector)

Check both sides of the multilink cable whether it is not damaged and correctly connected.

If you use external BDM interface like USB BDM Multilink, please ensure that ribbon cable is not damaged and you use correct pin position (You should check both ends ).

Please check whether MCU is hot - this typically signalize damaged MCU or short at connected load.

I would like to recommend test connection with the fresh new project.

If your project contains any data in the flash security field, the MCU may be secured. Please look at https://community.nxp.com/t5/CodeWarrior-Development-Tools/Usecure-S12Z-controller-via-debug-interfa...  document for more details.

Next thing to mention is whether you have downloaded and use the last drivers …. link bellow.

If nothing happens then another possibility for support is the manufacturer of the device www.pemicro.com.

 

Best regards,

Ladislav

0 件の賞賛
返信

1,757件の閲覧回数
GTM
Contributor I

I think my Multilink Universal Rev E is broken, because my Multilink Universal FX works just fine, by the way, in the same setup.

0 件の賞賛
返信