May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

跳至解决方案
888 次查看
aaronlee
Contributor V

May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
671 次查看
allen_willson
NXP Employee
NXP Employee

Aaron,

CAN requires a high accuracy clock source, usually 0.25% for high speed busses.

The internal oscillator is accurate to about +/- 1.3%, so it is not suitable to be used for CAN.

Please use an external crystal.

-arw

在原帖中查看解决方案

0 项奖励
回复
1 回复
672 次查看
allen_willson
NXP Employee
NXP Employee

Aaron,

CAN requires a high accuracy clock source, usually 0.25% for high speed busses.

The internal oscillator is accurate to about +/- 1.3%, so it is not suitable to be used for CAN.

Please use an external crystal.

-arw

0 项奖励
回复