May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

ソリューションへジャンプ
851件の閲覧回数
aaronlee
Contributor V

May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
634件の閲覧回数
allen_willson
NXP Employee
NXP Employee

Aaron,

CAN requires a high accuracy clock source, usually 0.25% for high speed busses.

The internal oscillator is accurate to about +/- 1.3%, so it is not suitable to be used for CAN.

Please use an external crystal.

-arw

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
635件の閲覧回数
allen_willson
NXP Employee
NXP Employee

Aaron,

CAN requires a high accuracy clock source, usually 0.25% for high speed busses.

The internal oscillator is accurate to about +/- 1.3%, so it is not suitable to be used for CAN.

Please use an external crystal.

-arw

0 件の賞賛
返信