May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

Jump to solution
790 Views
aaronlee
Contributor V

May I use internal oscillator in S12ZVCA for CAN bus 250Kbps or 500Kbps?

Labels (1)
0 Kudos
Reply
1 Solution
573 Views
allen_willson
NXP Employee
NXP Employee

Aaron,

CAN requires a high accuracy clock source, usually 0.25% for high speed busses.

The internal oscillator is accurate to about +/- 1.3%, so it is not suitable to be used for CAN.

Please use an external crystal.

-arw

View solution in original post

0 Kudos
Reply
1 Reply
574 Views
allen_willson
NXP Employee
NXP Employee

Aaron,

CAN requires a high accuracy clock source, usually 0.25% for high speed busses.

The internal oscillator is accurate to about +/- 1.3%, so it is not suitable to be used for CAN.

Please use an external crystal.

-arw

0 Kudos
Reply