Max3050 CAN communication with XEP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max3050 CAN communication with XEP100

1,250 Views
madhura_bhandig
Contributor I

Hello everyone,

I am working on CAN communication between two XEP100 controllers. I am using MAX3050 CAN IC. 

The resistance between CANH and CANL is to be 120 Ohm, but I am getting 167KOhm.

This is causing problem in communication, I am getting a dummy data in Rx side.

Please guide me regarding this.

Thanks in advance

Regards,

Madhura

0 Kudos
Reply
1 Reply

1,185 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

I'm not familiar with MAX3050 but I guess you should add an external 120ohm termination.

Regards,

Daniel

0 Kudos
Reply