MSCAN Module for MC9S12XEQ512 MAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSCAN Module for MC9S12XEQ512 MAL

3,985 Views
mohamedbouich01
NXP Employee
NXP Employee

Hi,

I would like to use the MC9S12XEQ512MAL to generate a CAN frame (without receive one). Indeed I have to to wake up an IC with a specific CAN frame.

I made several try without success......

I don't have the frame expected at MCU pin number 104 (txcan0).

 

Would like, please, help me on this issue ? Maybe you have a code ready to use to obtain the CAN frame with this version of S12X.

 

Many thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

3,855 Views
RadekS
NXP Employee
NXP Employee

Hi Mohamed,

The simple example code is in attachment.

More examples are for example here:

LAMA's S12XE unofficial examples ​

The “official” msCAN driver:

http://www.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_S12_DEVD.zip ​


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply