MSCAN Module for MC9S12XEQ512 MAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MSCAN Module for MC9S12XEQ512 MAL

3,991件の閲覧回数
mohamedbouich01
NXP Employee
NXP Employee

Hi,

I would like to use the MC9S12XEQ512MAL to generate a CAN frame (without receive one). Indeed I have to to wake up an IC with a specific CAN frame.

I made several try without success......

I don't have the frame expected at MCU pin number 104 (txcan0).

 

Would like, please, help me on this issue ? Maybe you have a code ready to use to obtain the CAN frame with this version of S12X.

 

Many thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

3,861件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Mohamed,

The simple example code is in attachment.

More examples are for example here:

LAMA's S12XE unofficial examples ​

The “official” msCAN driver:

http://www.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_S12_DEVD.zip ​


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信