MM9Z1_638 Isense input mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1_638 Isense input mode

ソリューションへジャンプ
1,791件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

 

is there a special bit to activate the differential mode of the ISense input?


regards

0 件の賞賛
返信
1 解決策
1,777件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

No, by setting the CMEN bit (when CMENM = 1) the differential mode is activated automatically, the current is measured by measuring the voltage drop over an external shunt resistor connected to ISENSEH and ISENSEL.

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
1,778件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

No, by setting the CMEN bit (when CMENM = 1) the differential mode is activated automatically, the current is measured by measuring the voltage drop over an external shunt resistor connected to ISENSEH and ISENSEL.

Best regards,

Tomas