MM9Z1_638 CAN Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1_638 CAN Bootloader

6,909件の閲覧回数
jtpark
Contributor IV

Hello,

MM9Z1_638 has CAN module.

Could you support CAN bootloader?

I checked it can be supported by VECTOR but it is not free.

 

Please help.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,987件の閲覧回数
gumu
Contributor V

@iggi  

Can't access AN3391SW.zip​ webpage, could you update a new websit?

Thanks!

0 件の賞賛
返信

5,226件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi J.T.,

Bootloader for S12Z derivatives (without CAN):

AN4723 S12Z MagniV Bootloader

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4723.pdf

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4723_SW.zip


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,131件の閲覧回数
Evgeniyy
Contributor I

Привет. Эти ссылки недоступны. Вы можете обновить ссылку?

0 件の賞賛
返信

5,226件の閲覧回数
iggi
NXP Employee
NXP Employee

Well, the CAN bootloader does not exist exactly for this device.

But you can re-use the one written for S12XE family which has the same S12MSCANV3 module integrated on the chip.

The application note AN3391 provides detailed information and SW project:

AN3391

AN3391SW.zip

Also some more additional information you can find here too:

Useful documents for building own CAN bootloader

So, this all is for free, but you would need to invest some effort to make the CAN bootloader for your application.

Regards,

iggi

0 件の賞賛
返信