MM9Z1_638 CAN Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1_638 CAN Bootloader

7,080 Views
jtpark
Contributor IV

Hello,

MM9Z1_638 has CAN module.

Could you support CAN bootloader?

I checked it can be supported by VECTOR but it is not free.

 

Please help.

Labels (1)
0 Kudos
Reply
4 Replies

4,158 Views
gumu
Contributor V

@iggi  

Can't access AN3391SW.zip​ webpage, could you update a new websit?

Thanks!

0 Kudos
Reply

5,397 Views
RadekS
NXP Employee
NXP Employee

Hi J.T.,

Bootloader for S12Z derivatives (without CAN):

AN4723 S12Z MagniV Bootloader

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4723.pdf

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4723_SW.zip


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,302 Views
Evgeniyy
Contributor I

Привет. Эти ссылки недоступны. Вы можете обновить ссылку?

0 Kudos
Reply

5,397 Views
iggi
NXP Employee
NXP Employee

Well, the CAN bootloader does not exist exactly for this device.

But you can re-use the one written for S12XE family which has the same S12MSCANV3 module integrated on the chip.

The application note AN3391 provides detailed information and SW project:

AN3391​

AN3391SW.zip​

Also some more additional information you can find here too:

Useful documents for building own CAN bootloader​

So, this all is for free, but you would need to invest some effort to make the CAN bootloader for your application.

Regards,

iggi

0 Kudos
Reply